Why We’ve Extended Inspection Intervals On 134 Parts (With More to Come)

September 17, 2019 | Author: Mike Beazley

At Honeywell Aerospace, we’re driving to make it easier and less time consuming for aircraft operators to maintain their fleets. That’s why we’re undertaking a comprehensive review of our entire product portfolio to assess extending recommend maintenance intervals.

The objective is to identify opportunities to safely extend the time between routine inspections or to provide alternate parts with more time between inspection, saving operators time and money. We’ve already identified 134 components as part of this effort, including parts used in certain cockpit, safety, navigation and sensor, and power systems.

Operators can find details on these interval changes in the service bulletins on MyAerospace (login required).

Several hundred additional parts used in Air Transport aircraft and Business Jets are now being evaluated and we expect to announce more maintenance interval extensions over the next two years.

In reviewing this second wave of components, we’ll follow the same process used on the first 134 parts, which includes a thorough analysis of operating data provided by the aircraft operators, coupled with R/O shop data and appropriate engineering analysis.

Approximately 93 percent of Honeywell produced components are designated for on-condition maintenance, which means routine inspections are not required and maintenance is done only if the part fails. When this portfolio review is completed that number is projected to grow to 95 percent. We’re also working to align service intervals on the remaining 5 percent with other major aircraft maintenance milestones, to make it even easier for aircraft operators to service our equipment.

Maintenance is one of an airline’s most important responsibilities and at Honeywell, we’re committed to making our products more reliable and easier to maintain.

Mike Beazley

Mike Beazley

Vice President of Global Technical Operations for Honeywell Aerospace

Comments



  • Guillermo Lozano Robledo

    Excellent initiative to save on scheduled maintenance (134 devices are many, and I know that more studies are still being carried out to increase this number of components), and extension of the life and revision of the components. In my life in aeronautics, for more than 15 years, I have a structure related to some Honeywell components and I know that they are high quality components, very precise and excellent finished equipment that give the confidence of functionality, and the certainty that they they will not fail Honeywell is a company with a great trajectory in Mexico, it is a company of the Future 100 that makes you want to belong with great enthusiasm and with the soul committed by the company.

    Reply